Part Number: ADS4249EVM
Other Parts Discussed in Thread: CDCE72010, , ADS4249
Hello,
I'm using the ADS4249EVM board. The board has a built-in CDCE72010 chip on it.
I currently use a 1000 MHz clock oscillator which is divided by the default value of the CDCE72010 which is 4 so I got 250 Mhz. clock to the ADC.
It is working well and I got a nice spectrum.
I would like to be able to change the sampling rate to 200 MHz. (i.e. clock divider of 5) or lower frequency. I see that the CDCE72010 is controlled by the FT245RL chip:
I tried to find a way to control the CDCE72010 chip from the ADS4249 EVM software but I did not find how.
Can you tell me how to control this chip?