I could not find any value for the input capacitance at the analog pins of the adc. As we havce a driver critical application and can drive only max 50pF i have to calculate all parasitc capacitive loads at the analog signal. Input resistance is given as 1MR, but the ESD protection could add some pF at the input pin. Does anyone know something about the expacted C-load ?
Thanks in advance, Ch.Merz