Hello-
Does the ADS1298 confrom to IEC60601-2-25 and/or 60601-2-27? In patricular the pace detection circuit...
Thanks, and Best Regards,
-Tim Starr
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello-
Does the ADS1298 confrom to IEC60601-2-25 and/or 60601-2-27? In patricular the pace detection circuit...
Thanks, and Best Regards,
-Tim Starr
Hi Tim,
The ADS1298 is a component which could be used in medical equipment. As I understand the IEC60601-2-25, this is a listing of requirements for the actual end equipment, not the individual components within that equipment and/or system. Pace detection could be done in software and/or hardware, but again - on the component level only, so there would be no applicable IEC or medical 'standard' to conform to in this case.
Hi Dave - Welcome to our forum!
As Tom mentioned, the ADS1298 chip alone will not make your system IEC-compliant. The datasheet mentions these standards because the device features and performances enables you to design an IEC-compliant system. A couple of the requirements involve guaranteeing patient safety and minimum signal resolution, which is achieved by the whole system, not just the ADS1298.
Unfortunately, IEC standards have to be purchased by the customer who is designing and certifying their system and TI does not have any documentation to provide additional guidance.
Best Regards,
Hi Ryan,
Thank you for getting back to me, that clarifies things a little better. I understand that the whole system needs to comply to the standard and that the ADS1298 alone will not make the system complaint. All of the other components state that they have been tested and met the standard. I was more wondering if by adding the ADS1298 to the system will it still pass the standard's tests. Which i believe you have answered this question "device features and performances enables you to design an IEC-compliant system." the data sheet did not specifically state that it the chip met IEC60601-2-25 that's way i was asking. I do have a copy of the standard and if i understand you correctly as long as i adhere to it in my design, the ADS1298 will be able to pass the tests? (granted that everything else is also up to standard)
Thank you again for the response,
Dave G.