This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8556: Difference for manufacture process between ADS8558

Guru 19645 points
Part Number: ADS8556
Other Parts Discussed in Thread: ADS8558,

Please let me confirm about difference between ADS8556 and ADS8558.

I think that ADS855x series is nearly function and the same manufacture process (and reliability), is it correct?

(Resolution and clock, etc are only differ)

※Background

Customer is already using ADS8558, and they want to use ADS8556 for next.

If ADS855x series is the same process, they can use and register ADS8556 very easily by their internal circumstance.

Best regards,

Satoshi

  • Hello,

    Correct, these devices are part of the same family, they are pin and software compatiple with each other. The customer should have no problem changing from the the ADS8558 to the ADS8556.
    Please let us know if there is any support you need.
    Regards
    Cynthia