Part Number: PGA300EVM-034
Hello,
when I select a Calibration file, I get an Error message: "The selected calibration file doesn't match with the GUI version..."
Pressing OK to continue the calibration, it seems to work: "OWI Configuration": no error - "OWI Actiovation": nothing to do because OWI is active (pressing next), reading of registers starts, but than the monitor is clear and the following error appears:
Unexpected Error occured during calibration
Error -20145 occurred at Error occured during interpolating values
Possible reason(s):
Analysis: Each independent variable must contain the same number of values as the dependent variable.
Try calibrating again
What can I do? I installed the latest version (3.5.1.0) from the GUI and I use the original ini-files...
Thanks for any help
Walter