Part Number: ADC12DJ3200EVM
Other Parts Discussed in Thread: LMX2582, LMK04828, ADC12DJ3200
When using the EVM GUI the register values for the LMX2582 do not all appear correct. For instance, when programming the EVM for 1500MSPS and JMODE0 the OUTA/B PD check boxes are always checked. Viewing Low Level register 46(0x2E) the PD bits are indeed 0 but are not broken out in the Field View section. If I look at 47(0x2F) the Field View shows the PD bits and indicate they are '1' but in the datasheet those are reserved bits set to '1'.
Also most of the time when a manual Read Register is issued, only for LMX2582, it returns all 1's and this is displayed in the LMX tab. I am exploring how the LMX gets programmed and these issues are making it difficult.
I am running windows 10 with a rev A EVM.
Thank you.