Part Number: DAC8750
Make a 4-20mA circuit in accordance with the circuit diagram in the manual. The unused pins are floating.
It is advisable to ask if the EN1 EN2 of ISO7631 is floating or connec
ted to the power supply.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC8750
Make a 4-20mA circuit in accordance with the circuit diagram in the manual. The unused pins are floating.
It is advisable to ask if the EN1 EN2 of ISO7631 is floating or connec
ted to the power supply.
Hi,
EN1 and EN2 are the enable pins for the isolation device. They should be either tied high or left floating to enable the device for successful communication with the DAC8750.
Thanks,
Garrett