Part Number: ADS805
I have the device configured for internal reference with a 0-5V input range. (SEL to ground; IN_N to Vref). I am using AC coupling with IN_P to 0.45V using a 2K to ground and 20K to +5V. When I power up the device IN_P goes to 0.45V as expected. When the clock starts IN_P rises to 0.6V. To me, that implies a sampling current of (0.6 - 0.45)/2K = 75uA. That is larger than I expected. Is this normal?