A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADS7830: How much current the internal reference can supply to the external circuitry?
The internal reference of the ADS7830 is not intended to drive external circuitry. What are you looking to do with the reference voltage outside of the ADC?
It is not recommended to use internal reference of ADS7830 to drive external circuit.
In your case you are using internal reference of the ADC for the external amplifier reference, the input bias current requirement from op-amp pin will not be much (Typically less than uA) and I think you should not see any performance degradation at 8 bit level.
If you have a long trace from ADC REF pin to op-amp pin then I would recommend to have local decoupling at op-amp pin.
Also please make sure ADC reference pin should have decoupling capacitor placed close to the pin (0.1uF to 1uF)