Other Parts Discussed in Thread: DAC8551, REF5025
Tool/software: Linux
I had some trouble in using DAC8531 to output an analog voltage to adjust the VCXO.
DAC8531 interfaced to MCU's SPI, Din------>MOSI,SCLK------->SCK,SYNC-------->GPIO, Vout------>Vcontrol(VCXO).sch as below:
I use mode 00, test the OUT:
Setting D =60000, write 1 times, VOUT output is incorrect, only 0.06V,It looks like no output;
Setting D =60000, cycle writes, Vout is not a fixed voltage.output jumps form 0V---2.1V.
When I setting Setting D =0xaaaa,The SPI sequence is as follows:
FIGURE 1 Pink------->SCLK, Yellow------>DATA
Code see attachment
Is there have any incorrect?
Tks!Best regards!