Part Number: ADS1256
Other Parts Discussed in Thread: DAC8532
Hi,
I bought a high-precision AD/DA board form Waveshare that uses the ADS1256 as ADC. They provide an example program to read the analog values but this goes rather slow.
Can someone help me with this, I'm using a Raspberry Pi in combination with the board.
Chip select is connected to pin 15 and when low it will select the ADS1256. Data ready is connected to pin 11. Want to receive an incoming signal with the ADS1256 24-bit and set the outcome as the variable for the ouput DAC 16-bit and at least 8kHz.
Hope someone can help or set me in the right direction.