Other Parts Discussed in Thread: ADS7953, ADS1158
Quick question is: can I use ADS7953 with +VA=3.3V and input channel voltage in range 0-3.3V? What do I need on REFP/REFM pins?
I'm confused by the datasheet and could not find any reference design for my needs.
I see REFP must be in the range 2.0-3.0V, but then I see that conversion uses 2xVref or Vref, whichever is smaller than +VA.
So with +VA=3.3V I can't use Vref=3.3V because it's too high, nor +VA=3.3/2=1.65V because it's too low.
So why does the datasheet specify that +VA can be in between 2.7V and 5.25V, if I can't use 3.3V with full scale conversion?
Can somebody clarify this a bit?
Thanks,
Paolo