Part Number: ADS54J66EVM
Other Parts Discussed in Thread: LMK04828, , ADS54J66
Tool/software: Linux
Hello,
I am having trouble accessing LMK04828 on ADS54J66EVM over SPI from Linux.
The board is connected over FMC on a ZCU102 Xilinx board. The SPI FMC pins are routed to Xilinx SPI controller. ADS54J66 is connected as SS 0 and LMK04828 as SS1.
I am able to successfully read and write ADS54J6T6 registers, however I can't seem to be able to write LMK04828.
I understand that the LMK04828 is configured as 3 wire SPI by default so I won't be able to read until I change the configuration to 4 wire SPI. (I may also need to add a 0-ohm resistor to R113 on the EVM board?) But before reading, I am trying to verify whether I can even write. Any attempts of register writes don't seem to be reflected if I switch to USB mode and read the registers using the ADS54Jxx GUI.
Any help will be appreciated.
Thanks,
Lenny