Part Number: PLABS-SAR-EVM-PDK
Other Parts Discussed in Thread: OPA320
Purchased a PLABS-SAR-EVM kit to use with the Precision Lab Pro seminar. Everything seems to work, except the range of the converted data. I have the PSi Controls set for 2 Vpp Amplitude, 1.5 V DC Offset, Single Ended Output. after clicking on Update, the sliders to the right show the proper 0.5V to 2.5V range. After pressing the Capture button, the graph and the Min and Max values are shown as 0.300V to 1.299V. I verified that the output signal of the PSI is a 2KHz 2 Vpp sign offset by 1.5V.
The unit looks like it was a returned/refurbished unit as all the static back had new anti-static stickers, but I could see the old ones.