Part Number: ADS8353EVM-PDK
Hi,
Just a confirmation about the EVM,
does ADS8353EVM-PDK comes with an AC adapter for 5V supply?
Best Regards
paddu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Paddu,
The ADS8353EVM-PDK evaluation kit powers up using the USB connection to the PC; and includes an on-board analog +5V supply, therefore it does not require (nor include) an AC adapter.
The controller in the evaluation kit connects to the PC USB port, and generates a +5.5V supply, which is then sub-regulated to +5V using a low noise linear regulator in the ADS8353EVM daughter board.
Please refer to the Power Supplies Section (Section 4, p.9) and the schematic (Section 7, p.35) of the ADS8353EVM-PDK Users Guide.
Thank you and Best Regards,
Luis