Part Number: ADC12DJ3200EVM
Other Parts Discussed in Thread: TSW14J57EVM, , ADC12DJ3200
Hi,
How to activate the Trigger Option in High Speed Data Converter Pro ver. 4.80?
I use ADC12DJ3200EVM rev.A + TSW14J57EVM rev. E.
Thank you,
Vladimir
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADC12DJ3200EVM
Other Parts Discussed in Thread: TSW14J57EVM, , ADC12DJ3200
Hi,
How to activate the Trigger Option in High Speed Data Converter Pro ver. 4.80?
I use ADC12DJ3200EVM rev.A + TSW14J57EVM rev. E.
Thank you,
Vladimir
Thank you, Jim.
I would like to know when the trigger mode will be implemented.
We need it as soon as possible.
Best Regards,
Vladimir
Hi Vladimir
I should be able to provide something that will enable Trigger Mode with your setup tomorrow.
Please let me know which ADC12DJ3200 JMODE you are using.
Also make sure you are using High Speed Data Converter Pro v4.80. The solution involves a patch that adds some files to that specific version of software.
Best regards,
Jim B
Hello Jim,
I'm using JMODE0, JMODE2 and High Speed Data Converter Pro v4.80.
Thank you,
Vladimir
Hi Vladimir
Ensure High Speed Data Converter Pro is not running and then install the following patch for v4.80:
/cfs-file/__key/communityserver-discussions-components-files/73/3343.HSDC-Pro-Patch-v4.80.02.zip
The file ADC12DJxx00_JMODE2_trig.ini has been added to the folder location below:
C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\14J57revE Details\ADC files
Several other supporting files will also be added.
In the Select ADC field choose "ADC12DJxx00_JMODE2_trig".
If this works for JMODE2, then you can create a new file ADC12DJxx00_JMODE0_trig.ini by comparing the existing ADC12DJxx00_JMODE0.ini file with the new JMODE2 file mentioned above and editing/adding as follows:
Trigger Input Polarity Selection = 1
Trigger Output Default State = 0
Trigger Output Pulse Width = 40
Sysref Based Master Slave Trigger = 0
Is Capture Trigger SMA = 1
I hope this is helpful.
Best regards,
Jim B
Hi Jim
I was able to enable the trigger mode. Now I'm checking this mode.
Thank you
Vladimir