Part Number: ADS7946
Are there any concerns with using the ADS7946 with a SCLK clock rate of 2-4 MHz? The processor that is controlling this ADC cannot run the SPI bus much faster than this, and a sample rate of 100k-200ksps is good enough for the application.
The data sheet provides a max clock rate, but not a minimum. There is information about running at lower sample rates, but this still assumes a 40 MHz SCLK.