This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1406EVM: TSW1406EVM vs TSW1400EVM

Part Number: TSW1406EVM

Hello,

I am currently using the TSW1400EVM board attached to our DAC board.  We were looking into downsizing to the 1406 board due to project reasons and for the fact that we don't use 90% of the components on the 1400 board.  The only problem we will encounter is the memory loss by downgrading to the 1406.  Is there any way to buy the 1406 board with the 512M 16-bit memory depth instead of the 64K 16-bit memory depth? This would be very beneficial to our application!

Thanks