Part Number: ADS1248
Other Parts Discussed in Thread: ADCPRO, ADS124S08
Dear TI Team,
I am designing the ADS1248 and have questions during the test.
There is a problem with the connection of the input.
I use AIN0 ~ AIN7 to connect, and I switch ON / OFF of AIN to confirm the value.
However, if the connection to AIN0 is lost, the value of the Output will be erroneous.
From AIN1 to AIN7, we confirmed that there is no problem even if the connection is broken.
If only AIN0 is disconnected, an error will occur.
It is necessary to check whether AIN0 is always connected.
Thanks.