Part Number: ADS1281
Hello,
Our customer use the ADS1281, have a question about clock input timing.
Refer to the Figure 42, the clock signal is input before DVDD.
But the absolute maximum ratings of the digital input is less than DVDD+0.3V.
Is the clock input timing of the figure 42 correct?
Should the customer input the clock after power on?
Best Regards,
Naoki Aoyama