Part Number: ADC12D1600RF
HI,
in the datasheet (6.1.2.5) regarding input clock jitter (Tjmax), there is a formula using 2^(N-1) where N is the ADC resolutions in bits.
my question is, does N in this device is 12 or should I look at the ENOB, where its mentioned that the effective number of bits is actually ~9. (looking at the datasheet tables and graphs for my input frequency and mode).
since my frequency is around 1300MHz , I get Tj=~15fSEC if N=12 and Tj=~120fSEC if N=9.
which is the correct calculation and why?
thanks