This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC34H84: FMC-DAC-ADAPTER REV-D pin configuration is not match with DAC34H84 Evaluation boards

Part Number: DAC34H84
Other Parts Discussed in Thread: FMC-DAC-ADAPTER

Deal All;

            I have brought DAC34H84 Evaluation board with FMC-DAC-ADAPTER for connecting with ZYNQ ZC702 boards. I have come across their pin connections, it seems that DAC having connectors with 180 pin and FMC-DAC-Adapter having 160 pins.

1) Is this boards is corrects or compatible with Xilinx Zynz ZC702 FPGA board?

2) is FMC-DAC-Adapter is compatible with DAC34H84 Evaluation board?

 Thanks and Regards

Imran Sheikh