Part Number: TSC200XSW-LINUX
Other Parts Discussed in Thread: TSC2007
Tool/software: Linux
Hi,
I use tsc2007 driver for my touchscreen on a raspberry. The raspberry runs on a 4.4.24-7+ linux kernel. I used tsc2007.c that I found in the kernel main line on gitHub. I then complied it directly on the pi and added it with depmod and modpropbe. Finally, I added a device_tree overlay that you can find here (that I created from the base here).
The touchscreen works mostly properly. I can calibrate it with ts_calibrate tool, and test it with ts_test. The last issue is the click event. I can not click any elements of my GUI, I can only move the cursor.
When I test my touchscreen with evtest, I see that the driver only triggers BTN_TOUCH event, while a mouse triggers BTN_LEFT. One way to do what I want is to modify the module to emit a BTN_LEFT instead of a BTN_TOUCH. But in kernel.org, it is said that : "
BTN_{MOUSE,LEFT,MIDDLE,RIGHT} must not be reported as the result of touch
contact. BTN_TOOL_<name> events should be reported where possible.
"
Is there a better way to do that ?
Thanks,
Nathanaël.