Part Number: ADC10065
Other Parts Discussed in Thread: THS4521
Dear all,
one of my AA is noticing high offset (after the conversion) and he thinks is due to some imbalance at the input of the ADC.
The ADC10065 is driven by a THS4521 op amp. The op amp and the ADC seats on 2 different boards. The offset is noticed also when a simple DC signal is connected to the ADC.
Up to now (this is an old project) there wasn't any offset issue and he thinks that the lot of ADC he has received has a different input impedance. He would add a matching resistor network to re-balance the impedance.
In the Datasheet there isn't any info onthe resisitve impedance of the input stage of the ADC. Are there any data available ? (typical and variations).
regards,
Domenico