We start using the ADS1299 EVB and have some question regarding the Bias.
KIT: ads1299 demo kit SLAU443 – MAY 2012 (lit num SBAS499).
- For doing internal BIAS TEST as indicated :
It is not clear what should I expect to receive. No indicative picture. I understand BIASIN pin uses internal BIAS of 2.5v. (AVDD+AVSS)/2 = 2.5v. So should I get 0V?
I am getting about 0.5V. Could you clarify ?
- I am using 6V for supply. I can also use 6v batteries as shown in the manual
Normal Electrode Test with differential inputs centered around 0 volt requires bipolar supplies of +/-2.5V. Is this supply generated on the demo board and just need to set jumpers or I should connect somehow bipolar supply externally. Please clarify specifically.