Other Parts Discussed in Thread: INA196,
Hey As I am working with 3 different sensor (like temperature, flow meter, pressure sensor) which is connected far away from 2 wire current loop receiver. I am checking the value from sensor and transmitter directly(with multimeter) first and after that while checking it from current loop receiver(with multimeter) the value is slightly lesser from the previous one
For Example:
I have temperature sensor and during 40 degree Celsius I should get the value of 8.266mA but I am getting 7.88mA similarly when temperature Is at 82 degree Celsius we should get value of 16.16mA but actual value is coming out to be 15.66mA
I am not able to understand where I am facing problem
Kindly how to overcome with this problem?