Tool/software: Code Composer Studio
HI , I've a trouble with ads1220 ,it receive clock and data even when cs pin is high . The converter work fine if it is connected alone ,but with others spi ic , i receive wrong data.
The microcontroller is TMC1294 ,
i've connected also a 100K pull up resistor to the cs pin .
Just for test i've tried to read the converter with the cs high and it doesen't send any data.(mean that the cs work fine)
ads1220 setting , continuos conversion mode. dataready is also monitored.
do you have any suggestion?
thanks best regards.