This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8775EVM: DAV8775 EVM Frist startup problems / basic adjustments

Part Number: DAC8775EVM


Hi,

i want to do raw trials over the windows evaluation program (seems to be a labview program).

I connected J2 to +24V and GND.

Which jumper connections have i to do to enable Output A for basic trials (voltage or current output)

When i start the labview program and i do a reset following changes inside the HMI are filled in:

Please could you give me some hints or troubleshooting details..

Thanks in advance