Other Parts Discussed in Thread: TVP5151
Hi,
Any one have registry setting for TVP5151 video decoder? I want to convert s -video input. If you have can you please share it?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Below are the basic register settings required for NTSC and PAL support. Use of the latest patch code which has various firmware improvements is highly recommended for your final application.
REG 00h = 01h // select s-video input
REG 03h = 09h // enable YCbCr data and clock outputs. Use 0Dh to also enable separate sync outputs
REG 0Dh = 47h // enable 8-bit 4:2:2 outut with embedded syncs (default).
Patch load application note:
http://focus.ti.com/lit/an/slea094/slea094.pdf
Latest patch code: