This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7760: -0.5 V source for AVSS

Part Number: DAC7760
Other Parts Discussed in Thread: LM7705

In continue to

We want to use DAC in 0-36V output range. So we need negative voltage source as low as possible to -0.5V. Because the output range of DAC has limited to 36V and each negative volt on AVSS lead to decrease maximum VOUT.

But all inductorless invertors working from 1.5V and required mirrored positive voltage http://www.ti.com/power-management/non-isolated-dc-dc-switching-regulator/buck-boost-inverting/charge-pump-inductorless/products.html#

So we should use at least 2 ICs - positive regulator + invertor or invertor + negative regulator. These solutions is not pretty.
At the same time all design and EVMs for DAC7760 provide solution for ±5/±15 V.

How TI recommend to implement 0-36V out? What should use do for -0.5V source?