This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J40EVM: ADS54J40EVM need US re-export licence required

Part Number: ADS54J40EVM


Is this EVM US re-export licence required?

if the parameters shown below are met or exceeded for the part  ADS54J40EVM with US ECCN 3A002.h

if US re-export license is required pls support written/email confirmation

MT applies ro 3A002.h when parameters in 3A101.a.2.b are met or exceeded 

3A101.a.2.b : Electrical input  type A-to D converter printed circuit boards or modules. having all of the following characteristics.

a.2.b.1 : Rated for operation in the temperature range frpm below -45C to above +80C

a.2.b.2 : Incorporation micro circuits identified in 3A101.a.2.a