Hello everybody,
i am working on a solution for a DSP-System using the ADC08D1520 RB. I want to use this RB because i have it anyway from previous projects.
The project is about controlling trigger voltages (On and Off Signals) for a gate driver, dependent on the respective voltage slopes sampled in the previous cycle.
The Task:
I want to sample two voltages in the range of up to 16V/ns. After sampling the Data, it should be processed on a FPGA which then sends the modulated trigger Signals via an isolation to a DAC.
Because i am not really sure about the possibility to program the on board virtex 4 FPGA, i want to send the ADC captured data to another FPGA where i can do the processing using Matlab.
After that i need to interface an SPI-Isolator which leads to a DAC.
The Question:
The FMC-Connector seems to be the right part to interface a external FPGA. Is there a way to do it this way? I didn't find anything about interfacing other hardware using the FMC-Port.
Is it possible to accomplish the task using the respective Hardware? For that i attached a Schematic to this post.
Thanks in advance,
Best Regards,
Benni