Please specify Vih max level of ADC12DJ3200
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ayesha
Which device pin specifically are you asking about?
The Vih and Vil levels for the CMOS inputs are listed in section 6.3 Recommended Operating Conditions.
Best regards,
Jim B
Hi Jim,
In section 6.3 Vih min is specified but we need the maximum limit for Vih. Can all the ADC control pins be directly connected to 1.8V CMOS bank of the FPGA or a buffer/level translator is required?
Regards,
Ayesha
Hi Ayesha
The Vih min is listed as 0.7V for the LVCMOS inputs. Any voltage at or above 0.7V will be recognized as a logic high.
The absolute maximum voltage that can be applied there is listed in table 6.1 as VA19+0.5V.
I recommend using a 1.8V bank from the FPGA for all of the ADC LVCMOS inputs.
Best regards,
Jim B