Part Number: DAC8871
Hi,
I'm not sure why, but my clock is pulled low when connected to the SCLK of the DAC
Image 1 shows the clock while connected to the DAC, image2 enlarges the clock and image3 shows while the clock is not connected to the SCLK of the DAC.
What am I doing wrong?
Connections are as followed:
Vout -> scope DGND -> ground
VCC -> +15V LDAC -> ground
Vss -> -15V SDI -> MOSI
AGND -> ground SCLK -> SCLK
VREFH-F -> =15V CS -> GPIO
VREFH-S -> nothing RST -> 3.3V
VREFL-S -> nothing RSTSEL -> VDD
VREFL-F -> -15V VDD -> 3.3V
(Clock should give 3.3V for high)