This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7846: How to connect the VREF pin 9

Part Number: ADS7846


I am using differenctial mode SER/DRF = 0

Should I connect VREF pin 9 to VCC pin 10?

if you have a schematic example will help alot

Thank you

Fausto Bartra

fbartra@tekran.com

416 449 3084

  • Hi Fausto,

    Apologies for the delay here on your query. Please review the 'REFERENCE INPUT' section of the datasheet starting on page 9, paying particular attention to the paragraph under Figure 5 (page 10) regarding the reference in differential mode. You should connect +REF to VCC in most circumstances.
  • Tom:

    thank you very much

    I have production on hold so I am under pressure to get this going

    I just have a couple of questions:

    1.- can you email me the eval board schematics for this device? (can't find it anywhere)

    2.- should I disable the PENIRQ while I am reading the data from this device?

    ( I am affraid it does affect the readings if it is enable, my clock is only 50KHZ)

    3.- Do you have any more information about pressure detection? (pen vs finger touch)

    Thanks a lot

    Fauisto Bartra