Part Number: ADS8638
Other Parts Discussed in Thread: ADS8634, PGA281, ADS1158, TINA-TI
Hi I would like to use ADS8638 to sample 6 channels of analog signal at a 1.5 kHz per channel (9000 kSPS in total) for a real time control application.
The section on Application Section in the datasheet is somehow confusing. According to the datasheet, "The ADS8634/8 employ a sample-and-hold stage at the input. An 8pF sampling capacitor is connected during sampling. This configuration results in a glitch at the input terminals of the device at the start of the sample". In continue, there is another section on "DRIVING ANALOG SIGNAL INPUT WITHOUT AN OPERATIONAL AMPLIFIER" on which I have the following question.
I filter the analog signals with a low pass filter (Cut-off frequency = 482 Hz, R = 1kohms, C = 0.33 uF). Do I still need to put in a buffering Op-Amp at the inputs before the filter?
Thanks,
-Amir