Part Number: ADS1263EVM-PDK
Other Parts Discussed in Thread: ADS1263, ADCPRO
Hi,
I'm having the DSP not ready issue. I was using the ADS1263 EVM kit since couples days now and it was properly working.
After changing the supply from +5V to ±5V, the DSP not ready issue appeared. Not sure the supply have any to do with this fault.
I tried to reinstall the ADCPRO with the ADS1263 plugin which reinstall automatically the MMB0 driver. This do not solved the issue.
I tried to reinstall manually the MMB0 driver as stated in other post without any success.
The NI-VISA USB Devices is listed in the device manager.
Any ideas?
Thanks
Olivier Bergeron