Part Number: ADS1158
Hello,
I'm using an ADS1158 ADC to readout 16 channels of 0-5V inputs, Vref is 5V, supplied by an REF5050 Source.
I'm not using an analog buffer between the internal MUX and the ADC.
My problem is the following:
If I set VREF at an AIN-Pin, an read out the data, I get 32767 (0x7FFF) counts at this channel, which means if I can beliebe the datasheet, that the voltage would be 1.06*VREF, which is in fact definitely not correct.
Corresponding to the datasheet the readout of the channel should be 0x7800.
VREF is really 5V, I checked this several times, with different Multimeters (for exmample an HP 34401A).
Have you any ideas why this discrepancy (0x7FFF vs. 0x7800) occurs?
Best regards