Hello there,
maybe a very simple question for some of You :)
We are using the 24bit ADS1220 Sigma-delta ADC, everything is basically working the way it should, now come the difficult tricky parts as we are doing some noise evaluations and stuff in our actual environment.
Principally we want to measure a single ended signal voltage coming from a transimpedance amplifier, so maybe from 0V = GND to 2Vpeak, but it can also be very low, as low as for example 1mV.
So we thought the PGA would come in handy to measure the really small and the really big signals.
So we tried the ADS1220 in different config settings and are now a bit confused about wheather to measure single ended ( = no PGA allowed, due to Common-mode restrictions, right?), or ( in our previous tests proven less noise ) differential mode measurments.
But now the tricky question: Is it still pseudo differential if we put GND on eg channel 1, and our real signal on channel 0, then we do a differential measurement from CH0 - CH1, is this allowed or is it the same thing as a simple single ended measurment for CH0 to GND???
Right now i am assuming it is the same as a single ended one, since internally the PGA will produce error results, since its range is not specified any more, right?
Thanks for reading and replies.
seb