This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131E04: External clock and sample rate

Part Number: ADS131E04

Hello!

I am using ADS131E04 to sample three devices. I am counting on the fact that with a 2.048 MHz external clock the sample rate should be exactly 4000 Hz, with the same accuracy.

Is that true, or should I expect some differences in the sample rate (say, 4000.032 Hz or so)?

Thanks in advance.

Stefano