Part Number: ADS1278
Other Parts Discussed in Thread: ADS1178, ADS1271
Hi,
We used ADS1278, REF=2.5V,
Now when the P and N terminals of the differential input are shorted together, the output value of the AD is around 0.1mv, and the perceived accuracy is a bit low. At the same time, we measured the EVM evaluation board, also in this order of magnitude.
Do not know what the reason is that the conversion accuracy is relatively low, how can we improve the conversion accuracy, the specific picture as shown below:
Thank you.