Part Number: ADS7952
Dear :
I have used the ADS7952 to sample 3.3V but the output only 2.5V , the REFP power supply by REF5025IDR (2.5V) and the VA supply +5V and i have config DI06 to Setting input voltage range 5V(range2) the input voltage below 2.5V can convert succesfully
Should i increase the vref voltage beyond 3.3V so it can sample 3.3V succesfully ?
In other words does it can sample 3.3V when Vref=2.5V VA=5V and select range2 ?
please help me , thanks