Hello Team,
1) Is there any problem with the operation below?
- DVCC,IOVDDA : Always supply 3.3V
- AVDD : supply 3.3V when during operation, and 0V when stopping operation
2) When power is supplied as below, is it no problem if the same voltage as DVDD or IOVDD is input to the digital pin(CS,DIN,SCLK,DOUT,DRDY,CLK,START/SYNC)?
- DVCC,IOVDDA : 3.3V
- AVDD : 0V
Best regards,
Kato