Part Number: ADS7042
Hi Team,
One of my customer consider ADS7042 for 1ch ADC.
Would you provide the feedback about below questions.
- Power supply scenario
They consider “AVDD=3.3V, DVDD=1.8V” or “AVDD=DVDD=1.8V”.
Each power supply are independent.
Case1) AVDD PMIC_3.3V / DVDD 1.8V
ADC input analog signal could be power on/off during normal operation.
Need to check, ADC input pin leakage voltage from AVDD when input signal power off case.
Case2) AVDD GNSS_3.3V / DVDD 1.8V
GNSS_3.3V could be power on/off during normal operation due to connected another block power reset.
Case3) AVDD 1.8V / DVDD 1.8V
ADC input analog signal could be power on/off during normal operation same as case #1.
There is no power sequence requiring, so they will decide case1 or case2 which better SNR than case3.
Is there any issue with these three different power supply case?
If case2 is possible (DVDD always on and AVDD on/off during operation), that is first priority. - Does it mean minimum 16 times SCK access required for calibration after power up?
- At least 16 times SCK toggling required during CS=low for SPI access, is this mean first access required 16 times SCLK and CS=low after power up and calibration complete correctly?
CS glitch signal should be prevent during power up? - How can customer know offset calibration is normal complete or abnormal case?
- At least 32 times SCK access required during normal operation for recalibration?
- If customer supply design AVDD=3.3V and DVDD=1.8V, there is power sequence between AVDD and DVDD.
DVDD 1.8V on first and AVDD 3.3V on after 5sec.
And only 3.3V AVDD 3.3V on/off during normal operation.
Is this possible supply design?
They will offset calibration access after AVDD on/off. - If AINN/P connected circuit power off while ADS7042 power on, AINM/P can detect voltage?
Is there any internal bias in ADS7042?
#6 and #7 quesiton related with #1.
Would you provide the feedback?
Thank you.
Best Regards,
Jade