Part Number: ADS1120
Dear Team,
Could you please help to review below schematic? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jim,
One thing I noticed but maybe isn't shown in the schematic snippets is that we recommend using approximately 47 ohm resistors in series with the digital connections for the serial interface. See section 9.1.1 on page 44 of the ADS1120 datasheet and Figure 72. Otherwise the connections to the ADS1120 look fine.
I do have a question about the bottom portion of the given schematic and the net NTC1_ADC as it is not shown where this net connects. I assume this is a microcontroller ADC input.
Best regards,
Bob B