This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA450Q1EVM: Ultrasonic sensor resonance tuning with fixed IFT

Part Number: PGA450Q1EVM
Other Parts Discussed in Thread: PGA450-Q1, PGA460

Hi,

I am using PGA450Q1-EVM with following circuit configuration.

Sensor frequency: 58kHz

Capacitance of sensor: Min 1200pf max 1800pf and nominal 1500pf

IFT (L): 4.2mH (Fixed value)

1. How can i calculate external capacitor to match the sensor resonance frequency. .As per theoretical calculation which sensor capacitance can i consider (Either Min or Max capacitance as per datasheet). 

2. Why theoretical calculated value always not matching with practical condition.How much tolerance acceptable?

  • Hi Arun,

    Responding to your questions:

    We do not have an accurate formula to calculate the value of the external matching capacitor. Section "8.2.2.1 Hardware" of the PGA450-Q1 datasheet shows equation-11, which is intended to approximate the ideal value of tuning capacitor based on the transformer's inductance and Butterworth-Van *** model equivalent of the transducer. We recommending using this calculated value as a starting point, but manually checking values within a +/- 500pF range from the calculated value. The difference in electrical versus mechanical resonance of a transducer will always counter performance of ring-decay or long range; it is up to the user to optimize which to improve and which to sacrifice based on min/max range requirements. This passive selection process is also described in the "PGA460 Ultrasonic Module Hardware and Software Optimization" ( www.ti.com/.../slaa732 ).

    Assuming nominal capacitance of the transducer, and fixed tuning capacitor value is selected, any deviation could be potentially be compensated by the configurable driver frequency. It is assumed that the ring-decay performance of transducer with a fixed tuning cap, but min or max sensor capacitor specification will always yield better performance compared to having no fixed tuning cap in place.

    Exact external passive matching can be difficult if the sensor capacitance drifts by +/-20%, but compensation through the driver frequency typically resolves this concern. Instead of always using 58kHz, you may find some transducer to have improved performance at 58.5kHz or 57.5kHz for example.