Hello community,
I hope you all doing good :-).
In my current project I am using the ADS1271 High Speed Data Converter. I am just confused about the clock ratio of the SPI Clock (f_SCLK) and the Master Clock (f_CLK). On page 25 of the datasheet one can read in section "SCLK (SPI Format) that for best performance the ratio of f_SCLK and f_CLK should be limited to 1, 1/2, 1/4,.... 1/2^(n+1) for n=0,1,2,3..... In my project I don't want to use a fixed sample rate so I want to make the master clock variable which leads with following equation fS=fCLK/512 to variable sample rates in SPI Mode. As micro controller I am using the STM32F429 which supports only fixed prescalers for the SPI. What happens if my ratio greater than 1, like 2,4,8... why I cannot achieve best performance if my SPI Clock is higher than my Master Clock ? After all, a higher SPI Clock would just read the bits faster out...
Thank you in advance !
best regards,
tuggy- bear :-)