We are using both the TVP5150 and THS8200 from TI to convert a compoiste NTSC signal to analog RGB. The video is converted however there is a purple hue on the RGB output, which indicates that the Green component is missing. When I put the THS8200 into the color bar test pattern I can see all of the colors so I know that there are no shorts on the board. I suspect that problem is with the TVP5150. Can you provide me with some clues on what the problem is?