have two questions about ADC IC (ADS1258MPHPTEP).
* Designed contents are as follows.
- 1.Analog Data (Input) -> 2.Inst-Amp (INA129MDREP) -> 3.ADC (ADS1258MPHPTEP) -> 4.Digital Data(Output)
* Inquiry 1. Offset occurs
- An offset of about 1.006 % occurs when the input analog data is compared with the output digital data.
(ex: Input: 1V -> Output: 1.006V, Input : 2V -> Output: 2.012V)
- I want to know why there is an offset and if there is a design problem.
* Inquiry 2. Remove Offset
- When designing the R-C filter on the outside and designing the feed-back of the MUX data by "ADC 43-44 pin-> R-C filter-> 41/42 pin"
The offset that occurred in Inquiry 1 has been removed.
- I want to know why the offset has been removed.
@ RC Filter Applied value: 130 Ohm, 100pF, Cut-Off Frequency: 6.18MHz