Part Number: ADS131A04
Hi all,
I have a question about Synchronous Master Mode. I connect the ADC like in figure 63( M0 pin to GND, ADC NDRDY is connected to DSP NCS).My DSP is in SPI Slave Mode. I would like to configure ADC registers after power up. If I understand correct, it means that I will shift out command word after DSP receive NCS. My question is when the ADC will initiate communication (pull down NDRDY) while ADC is not enabled(not written 0Fh to the ADC_ENA and no new data to pull NDRDY in normal way)?
P.S. I don’t have board(it is in production) and can’t check it by myself….